Self-calibrating Fisher easy-Drive 200R actuator is a more reliable and sustainable alternative to gas-operated actuators
MARSHALLTOWN, Iowa (Jan. 30, 2024) – Emerson has introduced the Fisher™ easy-Drive™ 200R Electric Actuator for use on Fisher butterfly and ball valves. When paired with these valves, the new actuator performs accurately and reliably under the extreme conditions found in many heavy industries, particularly oil and gas installations in cold remote locations. These actuator/valve assemblies increase uptime, improve performance, and reduce the risk of emissions posed by gas-operated systems locations.
Many pneumatic valve actuators installed in remote locations are operated using natural gas, but this technology releases atmospheric emissions every time the valve is actuated. Electric actuators address this issue by eliminating control-related emissions, but existing solutions have limitations, each of which is addressed by the 200R actuator.
• Easy installation & calibration: The 200R calibrates itself when a user simply clicks one button using the easy-Drive Configurator Software, provided free of charge with the actuator.
• Low energy usage: Operates on 11 to 30 VDC power and consumes less than 0.4 watts when in the holding position mode, making it suitable for use in applications without available utility power.
• Low temperature operation: Operates in temperatures as low as -40°C (-40°F), eliminating the need for a space heater in all but the most extreme temperature applications.
• Loss of power positioning: In the case of loss of power, the actuator can be driven to the user-defined position using its optional RPU-100 reserve power unit.
• Remote monitoring & configuration: Real-time monitoring of position, movements, cycles, travel time to position, and power loss available via a Modbus RTU serial interface.
The 200R is an extension of the easy-Drive actuator portfolio, which also includes actuator options for both globe and rotary valves. To learn more, please visit Emerson.com/fisher200r.
Media:
• Contacts: Emerson Global Media Contacts
Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via Twitter Facebook LinkedIn YouTube
About Emerson
Emerson (NYSE: EMR) is a global technology and software company providing innovative solutions for the world’s essential industries. Through its leading automation portfolio, including its majority stake in AspenTech, Emerson helps hybrid, process and discrete manufacturers optimize operations, protect personnel, reduce emissions and achieve their sustainability goals. For more information, visit Emerson.com.