eraaaaaaa
The mining pit is an inherently dangerous environment. The daily interaction between man and large, moving machinery creates an environment of ongoing risk. Add to that the unexpected shutdown of an electric rope shovel and the result is a real threat to both personnel safety and production goals. Everything on a shovel is subject to failure, and eventually you will experience a breakdown. The impact of that failure can be significantly reduced by monitoring key shovel components – the crowd, hoist, and swing drives. Emerson’s AMS 6500 has a proven history of monitoring for unique vibration characteristics found in rotating equipment – the same types found on many types of ore extracting assets, including the electric rope shovel.
Servers: Windows Server 2022 Standard, Windows Server 2022 Datacenter, Windows Server 2019 Standard, Windows Server 2019 Datacenter, Windows Server 2016 Standard, Windows Server 2016 Datacenter.
Workstations:
Windows 11 Professional, Windows 11 Enterprise, Windows 10 Professional x64, Windows 10 Enterprise x64, Windows 10 Enterprise LTSBServer/Portable Systems: 2.4 GHz 4-core processor or faster, 8 GB of RAM (minimum)
Workstations: 2.2 GHz 4-core processor or faster, 4 GB of RAM (minimum)