About Flame Detection Technology

About Flame Detection Technology

Find the right flame detector to help keep your people and facilities safe.

Electromagnetic Spectrum

Principles of Flame Detection

Flames emit electromagnetic radiation in the infrared (IR), visible light and ultraviolet (UV) wavelengths depending on the fuel source. Because some flames are invisible to the human eye, today’s flame detectors utilize optical technologies to detect flames. Optical flame-sensing technologies have been developed utilizing UV, UV/IR and multi-spectrum infrared to detect flames of differing fuel sources. These flame detection products rely on line-of-sight detection of the radiation emitted in the spectral bands to determine if a flame is real.

Meer lezen...
Klik om verder te gaan met lezen Principles of Flame Detection

Flame Detector Performance Criteria

Fuel Types

Consider whether the potential flame you are looking to detect will be hydrocarbon based or non-organic. With hydrocarbon flames, a combination of natural gases and oxygen produce carbon dioxide and water. This type of fire creates a UV signal reading at 0.2 microns and IR signal reading at 2.7 microns and 4.5 microns. Hydrogen flames only produce water molecules and therefore we do not see the same CO2 peak that a hydrocarbon flame is known to produce. Choosing a flame detector that's tuned to your fuel type and radiation intensity will provide more accurate flame detection. 

False Alarm Rejection

Environmental conditions like sunlight, lightning, hot objects like heat exchangers and other non-flame sources can cause false alarms. It's critical that a flame detector is able to distinguish between an actual fire and a false radiation source to prevent disruptive and costly false alarms. 

Coverage Area

Flame detection technologies effectively recognize a flame at different distances. It's important to utilize a flame detector that can operate within your required detection range. To improve the odds of successful flame detection, flame detectors are often placed so that their detection coverages overlap.

Optical flame detectors also have a “field of view”, similar to the lens on a camera. Taking the field of view range into account will help you determine how many flame detectors are needed to cover an installation or a specific area within the installation.

Understanding Flame Detector Technologies

Ultraviolet/Infrared (UV/IR) Flame Detectors

UV/IR flame detectors combine a UV optical sensor (0.18 – 0.26 μm range) with an IR sensor (2.5 – 3.0 μm range) designed to detect water vapor from hydrogen and hydrocarbon combustion. The combined UV/IR flame detector mitigates the drawbacks of a straight UV detector so it can be used outdoors, but with a slightly slower response time. Detection range may be reduced by heavy smoke. 

Multi-Spectrum Infrared (MSIR) Flame Detectors

MSIR multi-spectrum hydrogen and hydrocarbon flame detectors zero-in on infrared spectral regions between 2.0 – 5.0 μm to detect water and carbon dioxide emissions. The hot water band is particularly useful for detecting hydrogen fires, the flames of which are practically imperceptible in the visible light range. This type of flame detector has a long range and high immunity to smoke and false alarms.

MSIR multi-spectrum hydrocarbon flame detectors use the infrared spectral region of 4.0 – 5.0 μm to detect carbon dioxide emissions produced by hydrocarbon fires, but with no sensitivity to water vapor. This type of flame detector can detect fuel and gas fires at long ranges and has a high immunity to false alarms, but cannot recognize hydrogen fires.

Other Flame Detectors

Additional flame detector technologies that depend on line-of-sight radiation include:

  • Ultraviolet (UV) Flame Detectors
  • Single Infrared (IR) Flame Detectors
  • Visual Flame Detectors
Voor gebruik van deze website moet JavaScript worden ingeschakeld.