After grinding in the ball mill, fragments of ore remain that are too large to pass through the screen to the next phase. These fragments, along with foreign matter that can include broken balls from the mill, are ushered to the rejects line. Valves isolating these lines must provide zero leakage shutoff to prevent valuable water loss, while also being robust enough to resist severe impact damage.
The following products are capable of providing zero leakage shutoff of ball mill reject lines. They are also engineered to resist heavy impact damage and extend the uptime of your mill.
Sergei Mishin, measurement solutions sales director OEM Europe, explains how automation technology is essential to optimised, precise and safe production of anodes, cathodes and electrolytes. Global electric vehicle (EV) sales are growing and accounted for 10% of all new cars sold in 2022, but reports suggest that EV sales must increase to approximately 60% …
read morePresenting at the Emerson Exchange EMEA 2024, Juan Rodriguez, process control supervisor at Poderosa Mining Company, outlined how the implementation of magnetic flow meters has helped to boost energy efficiency and gold recovery. Poderosa Mining is a gold processing company located in the province of Pataz, almost 320 km from the city of Trujillo, in Peru. At …
read moreDownload this whitepaper for ways to drive safer, more efficient & more sustainable mining operations with edge controllers.
read more